Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

1,596件の閲覧回数
KojiTajima
Contributor II

Hi,

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

lazycast: https://github.com/homeworkc/lazycast

 

I was able to get the lazycast using the wget command, but when I run make I get a message 

like "ld: cannot find -lavformat" and the build doesn't complete properly.

Is it possible to get the library using apt / apt-get? If you can, please tell me the command sequence.

 

Best regards,

KojiTajima

0 件の賞賛
返信
3 返答(返信)

1,579件の閲覧回数
KojiTajima
Contributor II

Hi, joanxie

Thank you for your reply.

However, I looked at the HowTo page for advice and searched for the local.conf file but couldn't find it.

        # find / -name local.conf

The Linux image I'm using is "Linux imx8mqevk 5.15.5" downloaded from the NXP site. Is this Linux image not possible?

 

KojiTajima

0 件の賞賛
返信

1,551件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you need to build the yocto bsp source code, then find local.conf under <build folder>/conf

 

0 件の賞賛
返信

1,592件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信