Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

1,692 次查看
KojiTajima
Contributor II

Hi,

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

lazycast: https://github.com/homeworkc/lazycast

 

I was able to get the lazycast using the wget command, but when I run make I get a message 

like "ld: cannot find -lavformat" and the build doesn't complete properly.

Is it possible to get the library using apt / apt-get? If you can, please tell me the command sequence.

 

Best regards,

KojiTajima

0 项奖励
回复
3 回复数

1,675 次查看
KojiTajima
Contributor II

Hi, joanxie

Thank you for your reply.

However, I looked at the HowTo page for advice and searched for the local.conf file but couldn't find it.

        # find / -name local.conf

The Linux image I'm using is "Linux imx8mqevk 5.15.5" downloaded from the NXP site. Is this Linux image not possible?

 

KojiTajima

0 项奖励
回复

1,647 次查看
joanxie
NXP TechSupport
NXP TechSupport

you need to build the yocto bsp source code, then find local.conf under <build folder>/conf

 

0 项奖励
回复

1,688 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复