Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

1,603 Views
KojiTajima
Contributor II

Hi,

Is it possible to build and run the lazycast obtained from github on Linux imx8mqevk 5.15.5?

lazycast: https://github.com/homeworkc/lazycast

 

I was able to get the lazycast using the wget command, but when I run make I get a message 

like "ld: cannot find -lavformat" and the build doesn't complete properly.

Is it possible to get the library using apt / apt-get? If you can, please tell me the command sequence.

 

Best regards,

KojiTajima

0 Kudos
Reply
3 Replies

1,586 Views
KojiTajima
Contributor II

Hi, joanxie

Thank you for your reply.

However, I looked at the HowTo page for advice and searched for the local.conf file but couldn't find it.

        # find / -name local.conf

The Linux image I'm using is "Linux imx8mqevk 5.15.5" downloaded from the NXP site. Is this Linux image not possible?

 

KojiTajima

0 Kudos
Reply

1,558 Views
joanxie
NXP TechSupport
NXP TechSupport

you need to build the yocto bsp source code, then find local.conf under <build folder>/conf

 

0 Kudos
Reply

1,599 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply