Is eCSPI hardware identical between i.MX processors?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is eCSPI hardware identical between i.MX processors?

跳至解决方案
2,467 次查看
michael_stanger
Contributor I

Is the eCSPI hardware within the i.MX8 identical to previous i.MX7/6 processors?
If the hardware is the same, are the software drivers also therefore identical for each processor?

The reason I ask is that I'd like to characterise the performance of the eCSPI interface on an i.MX8M, but presently only have an i.MX7D development board available. If I can make use of the eCSPI hardware/software on the i.MX7D and be confident that it's representative of the i.MX8M eCSPI then that'd save us some time.

Cheers,
Michael

标记 (5)
0 项奖励
回复
1 解答
2,225 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michael

you are right i.MX8M eCSPI module is the same as in i.MX6/7.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,226 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michael

you are right i.MX8M eCSPI module is the same as in i.MX6/7.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------