Compatibility with both 1 GB and 2 GB DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatibility with both 1 GB and 2 GB DDR

825 Views
deexithamba
Contributor III

Hello,

I have been working on custom boards which is based on i.MX6DP, here we have boards with both 1 GB and  2 GB DDR. We have built seperate binaries for both the variants . My question is can we have the same set of binaries which can work with both 1 GB and 2 GB DDR to bring up Android Nougat on the custom board??!! If so, can you please tell me where exactly to look into!!

Thanks and regards,

Deexith V 

Labels (3)
0 Kudos
Reply
1 Reply

722 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deexith 

size is defined in uboot/../configs/mx6sabresd.h board file with parameter

#define PHYS_SDRAM_SIZE

ddr calibration settings are defined in uboot/..mx6sabresd/mx6qp.cfg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply