Is documentation availible for the i.MX8M Mini ASRC Block

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is documentation availible for the i.MX8M Mini ASRC Block

跳至解决方案
1,706 次查看
mobrien
Contributor II

Figure 13-90 on page 4174 of Document Number: IMX8MMRM Rev. 2, 08/2019 - the i.MX 8M Mini Applications Processor Reference Manual shows a diagram of the SPDIF clocking that includes an Asynchronous Sample Rate Converter (ASRC) block.  It also states that the SPDIF Rx clock is sent to the ASRC.  But the ASRC is not mentioned anywhere else in the document and I could not find any other documentation on how to enable and use the ASRC. Is there an ASRC availible on this IC? If so could we get some documentation on how to use it?

pastedImage_1.png

0 项奖励
回复
1 解答
1,623 次查看
mobrien
Contributor II
0 项奖励
回复
2 回复数
1,624 次查看
mobrien
Contributor II

Thanks Igor

0 项奖励
回复
1,623 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michael

you are right, i.MX8M Mini has not ASRC module and it is not mentioned

in any documents available on i.MX 8M Mini Applications Processor | Arm Cortex A53/M4 | 1080P display | NXP 

Only reference on page 4174 seems as misprint.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复