Is documentation availible for the i.MX8M Mini ASRC Block

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is documentation availible for the i.MX8M Mini ASRC Block

ソリューションへジャンプ
1,598件の閲覧回数
mobrien
Contributor II

Figure 13-90 on page 4174 of Document Number: IMX8MMRM Rev. 2, 08/2019 - the i.MX 8M Mini Applications Processor Reference Manual shows a diagram of the SPDIF clocking that includes an Asynchronous Sample Rate Converter (ASRC) block.  It also states that the SPDIF Rx clock is sent to the ASRC.  But the ASRC is not mentioned anywhere else in the document and I could not find any other documentation on how to enable and use the ASRC. Is there an ASRC availible on this IC? If so could we get some documentation on how to use it?

pastedImage_1.png

0 件の賞賛
返信
1 解決策
1,515件の閲覧回数
mobrien
Contributor II
0 件の賞賛
返信
2 返答(返信)
1,516件の閲覧回数
mobrien
Contributor II

Thanks Igor

0 件の賞賛
返信
1,515件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michael

you are right, i.MX8M Mini has not ASRC module and it is not mentioned

in any documents available on i.MX 8M Mini Applications Processor | Arm Cortex A53/M4 | 1080P display | NXP 

Only reference on page 4174 seems as misprint.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信