Hello,
Release notes of L1.14.98_2.3.0 Yocto BSP do not mention NAND boot support for i.MX8M Nano. Can you please update which BSP release is going to support this feature.
Thanks a lot.
Hello Felix,
Unfortunately since the EVK from the moment does not have a NAND Flash we do not have a plan to add the support to the BSP, nevertheless since it is under preproduction the i.MX8Nano, I can provide your suggestion to our team, so they can this in consideration.
Best Regards,
TIC Support Team
Hello,
When can I find NAND flashing instructions for i.MX8MQ or i.MX8MM ? These processors do have EVK boards with NAND flash and NAND support in kernel and u-boot.
Thanks.
Felix.