Is a tamper detection pin enabled when it is not used as GPIO?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is a tamper detection pin enabled when it is not used as GPIO?

1,613 次查看
Hirotoshi_Sato
Contributor II

Hi, I would like to know about TAMPER_PIN_DISABLE.

I use i.mx6ull CPU, so I referenced IMC6ULLRM.pdf

According to the manual,  definition of TAMPER_PIN_DISABLE[1:0] are as following :

        00 - enabled, TAMPER0-9 used as TAMPER detection pins.

        01 - disabled, TAMPER2-4 and TAMPER7-9 used as GPIO.

        10 - disabled, TAMPER0-1 and TAMPER5-6 used as GPIO.

        11 - disabled, TAMPER0-9 used as GPIO.

 (these are copied from Yuri's answer at mx6ul tamper pin to gpio  )

When I did "fuse read 0 3", I got 10 at [21:20].

It means that  TAMPER0-1 and TAMPER5-6 used as GPIO.

How about TAMPER2-4 and TAMPER7-9?

Do they work as tamper detection pins?

"enabled" is written only when fuse is 00, so I confused.

标签 (4)
0 项奖励
回复
2 回复数

1,366 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hirotoshi

in i.MX6ULL Tamper0 - 9 can not be used as tamper pins,

they are disabled via fusing during production. Can be used only as GPIOs.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,366 次查看
Hirotoshi_Sato
Contributor II

Thank you very much for your quick answer.

Do you intend that we can not transit RUN mode from SNVS mode?

Actually now my board can not run whatever I do after shutdown by "poweroff" command.

Only solution I found is removing CPU from my board and reconnect it.

I think my board entered SNVS mode even though there are no tamper pins.

May that case possible? If so, I think I have to remove VDD_SNVS_IN in order not to enter SNVS mode.

0 项奖励
回复