Interfacing KSZ9477 switch to imx8mp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interfacing KSZ9477 switch to imx8mp

2,262 次查看
vinay_hasyagar
Contributor III

Hello,

We are using KSZ9477 switch in our design which is interfaced with imx8m plus SoC. The KSZ9477 port6 (RGMII) is connected to eqos MAC of imx8M plus. The switch is made to configure using MDIO mode. It is also mapped in the device tree. After OS gets booted, if we see the ethernet interfaces then we are able to see eth1 is listed. In the dmesg, I can see imx-dwmac driver is also loaded properly. There is one more external phy which is connected to FEC MAC of imx8m plus which is working properly.

The issue is, the IP is not getting assigned to eth1. Do I need to add any configuration with respect to KSZ9477? Please find the device tree mapping of KSZ9477.

&eqos {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rgmii";
phy-handle = <&ethphy0>;
status = "okay";

mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;

ethphy0: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <1>;
eee-broken-1000t;
rtl821x,aldps-disable;
rtl821x,clkout-disable;
};
};

Please find the below block diagram which tells how switch is connected

vinay_hasyagar_1-1682340774303.png

The path RJ45--> KSZ9477--->KSZ9131(external phy)--->IMX8M plus is working.

The path RJ45--> KSZ9477--->IMX8M plus is not working because no IP address is getting assigned. Please tell me whether I need to add any configuration in device tree.

 

Thanks

0 项奖励
回复
3 回复数

2,248 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please check to this thread Using KSZ9031 PHY On i.MX8MM and L5.4.24_2.1.0, to use it as a reference.

Best regards.

0 项奖励
回复

2,205 次查看
vinay_hasyagar
Contributor III

Hi @JorgeCas 
Thank you for your reply. I went through the steps mentioned in the link and added the same thing. But that did not help. The product mentioned in the link is a phy and not an ethernet switch.

Thanks

0 项奖励
回复

2,188 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Researching a little bit more, I found that there is no limitation for EQOS controller to implement the configuration with the switch. But since this is not part of the default BSP, it is up to the customer to make the integration. NXP BSP offers basic enablement features.

Best regards.

0 项奖励
回复