Interfacing 12-bit camera with IMX6 EVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interfacing 12-bit camera with IMX6 EVM

783 次查看
adityanagal
Contributor III

My target board based on IMX6Solo is under design. Meanwhile , I need a IMX6 EVM with which I can interface 12 bit parallel camera . Any EVM supports 12- bit camera . I checked few EVM's , I could see 8 bit and 10 bit camera connectors over EVM . Can I do something for the 12-bit Camera ? Any suggestions.

0 项奖励
回复
1 回复

634 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

it may be useful to check Table 67. Camera Input Signal Cross Reference,

Format, and Bits Per Cycle i.MX6SDL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复