Interfacing 12-bit camera with IMX6 EVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing 12-bit camera with IMX6 EVM

792 Views
adityanagal
Contributor III

My target board based on IMX6Solo is under design. Meanwhile , I need a IMX6 EVM with which I can interface 12 bit parallel camera . Any EVM supports 12- bit camera . I checked few EVM's , I could see 8 bit and 10 bit camera connectors over EVM . Can I do something for the 12-bit Camera ? Any suggestions.

0 Kudos
Reply
1 Reply

643 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

it may be useful to check Table 67. Camera Input Signal Cross Reference,

Format, and Bits Per Cycle i.MX6SDL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply