I see in the documentation that while the iMX6DL is in deep sleep, only keypad, GPIO, and SNVS will wake it up. But the question is if any of the GPIO interrupts is wake up capable or only some of them, like those listed as GPIO1 0-7 / INT0-7.
Thanks.
Ismael.
Hi Ismael
yes any GPIO interrupt is capable to wake up
from low power modes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------