Input timing in DDR mode with loopback DQS sampling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Input timing in DDR mode with loopback DQS sampling

ソリューションへジャンプ
2,497件の閲覧回数
goto11
Contributor III

Hello,

 

I have two questions about QuadSPI's Input timing in DDR mode with loopback DQS sampling.
No1
Is it a mode that can be used with serial flash without DQS?
No2
Can the QSPI_A_DQS (EPDC1_DATA04) pin be open when used in this mode?
Or does the QSPI_A_DQS (EPDC1_DATA04) pin connect to any pin?

 

Regards,

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
2,492件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,493件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

0 件の賞賛
返信