Input timing in DDR mode with loopback DQS sampling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Input timing in DDR mode with loopback DQS sampling

跳至解决方案
2,487 次查看
goto11
Contributor III

Hello,

 

I have two questions about QuadSPI's Input timing in DDR mode with loopback DQS sampling.
No1
Is it a mode that can be used with serial flash without DQS?
No2
Can the QSPI_A_DQS (EPDC1_DATA04) pin be open when used in this mode?
Or does the QSPI_A_DQS (EPDC1_DATA04) pin connect to any pin?

 

Regards,

Goto

标签 (1)
0 项奖励
回复
1 解答
2,482 次查看
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,483 次查看
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

0 项奖励
回复