Input timing in DDR mode with loopback DQS sampling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input timing in DDR mode with loopback DQS sampling

Jump to solution
2,498 Views
goto11
Contributor III

Hello,

 

I have two questions about QuadSPI's Input timing in DDR mode with loopback DQS sampling.
No1
Is it a mode that can be used with serial flash without DQS?
No2
Can the QSPI_A_DQS (EPDC1_DATA04) pin be open when used in this mode?
Or does the QSPI_A_DQS (EPDC1_DATA04) pin connect to any pin?

 

Regards,

Goto

Labels (1)
0 Kudos
Reply
1 Solution
2,493 Views
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
2,494 Views
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   It is possible to use DDR QSPI flash without DQS, assuming
the loopback. Add 18pf on the DQS pin.

Regards,
Yuri.

0 Kudos
Reply