Imx8mm cannot connect to wifi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8mm cannot connect to wifi

2,044 Views
fu_qiang
Contributor II

Debug ap6255 chip on the board of IMx8mm. At present, the system is Yocto and the kernel version is 4.1.98. Only after configuring the device tree, wifi can be pulled up.But I found an error using WPA_supplicant when Connecting to wifi. Do I need to add another CONFIG or formula?Here is the error reporting part .thanks

root@imx8mmevk:/# wpa_supplicant -B -i wlan0 -c /etc/wpa_supplicant.conf
Successfully initialized wpa_supplicant
rfkill: Cannot open RFKILL control device
rfkill: Cannot get wiphy information
root@imx8mmevk:/#

0 Kudos
Reply
1 Reply

1,962 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fu

for wpa_supplicant usage one can look at latest wifi Linux Manual on link

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply