DDR register configuration on i.MX6 Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR register configuration on i.MX6 Quad

1,244 Views
rameshasp
Contributor IV

Hello Sir,

Currently i am using i.MX6 quad processor and DDR part number is MT41K256M16TW-107 IT:P, in this data rate is 1866 but DDR script file Memory type i am able to see maximum DDR3-1600. 

could you help me if i choose memory type DDR3-1600 is this correct, can i use this calibration value for my uboot image.

Please help me this is very urgent.

Advance thanks,

Ramesha  SP

Labels (1)
Tags (1)
2 Replies

1,214 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesha

 DDR3-1600 selection is correct, one can sellect 1600 grade for 1866 grade design.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,214 Views
rameshasp
Contributor IV

Thanks for your quick reply Igor.

0 Kudos
Reply