Imx8mm cannot connect to wifi

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx8mm cannot connect to wifi

2,042 次查看
fu_qiang
Contributor II

Debug ap6255 chip on the board of IMx8mm. At present, the system is Yocto and the kernel version is 4.1.98. Only after configuring the device tree, wifi can be pulled up.But I found an error using WPA_supplicant when Connecting to wifi. Do I need to add another CONFIG or formula?Here is the error reporting part .thanks

root@imx8mmevk:/# wpa_supplicant -B -i wlan0 -c /etc/wpa_supplicant.conf
Successfully initialized wpa_supplicant
rfkill: Cannot open RFKILL control device
rfkill: Cannot get wiphy information
root@imx8mmevk:/#

0 项奖励
回复
1 回复

1,960 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fu

for wpa_supplicant usage one can look at latest wifi Linux Manual on link

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复