Imx6 - chain of trust implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 - chain of trust implementation

2,279 次查看
DipinPK
Contributor II

Hi all,

I have implemented secure boot solution for our device. So, single public is used to verify both signed uboot and signed kernel.

But I need to implement chain of trust like below diagram

DipinPK_0-1612257450198.png

Here every component is verified by its unique public key that's embedded on the previous binary.

Can you help me to do that.

Thanks in advance

 

Regards

Dipin

 

 

0 项奖励
回复
4 回复数

2,269 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复

2,254 次查看
DipinPK
Contributor II

I have already implemented the secure boot feature. But need to implement the chain of trust. Using FIT images.

Can you suggest me some method for that?

标记 (1)
0 项奖励
回复

2,212 次查看
Yuri
NXP Employee
NXP Employee

@DipinPK 
Hello,

  we do not example with i.MX6 FIT image, sorry.

Regards,
Yuri.

0 项奖励
回复

2,228 次查看
DipinPK
Contributor II

What is FIT image how to create FIT images for imx6 processors

0 项奖励
回复