IMX6ULLEVK core-image on Zeus distribution fails to build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULLEVK core-image on Zeus distribution fails to build

813 Views
omerg
Contributor I

Im trying to build an image for IMX6ULLEVK but it seems the bitbake returns an error, i followed the guide on the product page regarding the 5.4 one, but it seems it seems an image cant be built bellow is the log file error i received:

 

ERROR: linux-imx-5.4-r0 do_compile: oe_runmake failed
ERROR: linux-imx-5.4-r0 do_compile: Execution of '/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/temp/run.do_compile.9943' failed with exit code 1:
GEN Makefile
scripts/kconfig/conf --syncconfig Kconfig
GEN Makefile
CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/atomic/check-atomics.sh
sha1sum not available, skipping atomic header checks.
CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/checksyscalls.sh
CHK include/generated/compile.h
Kernel: arch/arm/boot/Image is ready
Kernel: arch/arm/boot/zImage is ready
GEN Makefile
scripts/kconfig/conf --syncconfig Kconfig
make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-usb-certi.dtb'. Stop.
/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:1246: recipe for target 'imx6ull-14x14-evk-usb-certi.dtb' failed
make[1]: *** [imx6ull-14x14-evk-usb-certi.dtb] Error 2
/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:179: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/temp/log.do_compile.9943
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E zImage CC=arm-poky-linux-gnueabi-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0=/usr/src/debug/linux-imx/5.4-r0 -fdebug-prefix-map=/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0=/usr/src/debug/linux-imx/5.4-r0 -fdebug-prefix-map=/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot= -fdebug-prefix-map=/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source=/usr/src/kernel LD=arm-poky-linux-gnueabi-ld.bfd LOADADDR=0x10008000
| GEN Makefile
| scripts/kconfig/conf --syncconfig Kconfig
| GEN Makefile
| CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/atomic/check-atomics.sh
| sha1sum not available, skipping atomic header checks.
| CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/checksyscalls.sh
| CHK include/generated/compile.h
| Kernel: arch/arm/boot/Image is ready
| Kernel: arch/arm/boot/zImage is ready
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk.dtb
| GEN Makefile
| scripts/kconfig/conf --syncconfig Kconfig
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk-btwifi.dtb
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk-btwifi-oob.dtb
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk-emmc.dtb
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk-gpmi-weim.dtb
| NOTE: make -j 18 HOSTCC=gcc -isystem/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -L/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E imx6ull-14x14-evk-usb-certi.dtb
| make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-usb-certi.dtb'. Stop.
| /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:1246: recipe for target 'imx6ull-14x14-evk-usb-certi.dtb' failed
| make[1]: *** [imx6ull-14x14-evk-usb-certi.dtb] Error 2
| ERROR: oe_runmake failed
| /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:179: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work/imx6ullevk-poky-linux-gnueabi/linux-imx/5.4-r0/temp/run.do_compile.9943' failed with exit code 1:
| GEN Makefile
| scripts/kconfig/conf --syncconfig Kconfig
| GEN Makefile
| CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/atomic/check-atomics.sh
| sha1sum not available, skipping atomic header checks.
| CALL /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/scripts/checksyscalls.sh
| CHK include/generated/compile.h
| Kernel: arch/arm/boot/Image is ready
| Kernel: arch/arm/boot/zImage is ready
| GEN Makefile
| scripts/kconfig/conf --syncconfig Kconfig
| make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-usb-certi.dtb'. Stop.
| /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:1246: recipe for target 'imx6ull-14x14-evk-usb-certi.dtb' failed
| make[1]: *** [imx6ull-14x14-evk-usb-certi.dtb] Error 2
| /home/dev/zeus-imx-yocto-bsp/build-fb/tmp/work-shared/imx6ullevk/kernel-source/Makefile:179: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/dev/zeus-imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2161 tasks of which 2058 didn't need to be rerun and 1 failed.

 

Labels (2)
0 Kudos
Reply
0 Replies