Imx6 - chain of trust implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 - chain of trust implementation

2,218件の閲覧回数
DipinPK
Contributor II

Hi all,

I have implemented secure boot solution for our device. So, single public is used to verify both signed uboot and signed kernel.

But I need to implement chain of trust like below diagram

DipinPK_0-1612257450198.png

Here every component is verified by its unique public key that's embedded on the previous binary.

Can you help me to do that.

Thanks in advance

 

Regards

Dipin

 

 

0 件の賞賛
返信
4 返答(返信)

2,208件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信

2,193件の閲覧回数
DipinPK
Contributor II

I have already implemented the secure boot feature. But need to implement the chain of trust. Using FIT images.

Can you suggest me some method for that?

タグ(1)
0 件の賞賛
返信

2,151件の閲覧回数
Yuri
NXP Employee
NXP Employee

@DipinPK 
Hello,

  we do not example with i.MX6 FIT image, sorry.

Regards,
Yuri.

0 件の賞賛
返信

2,167件の閲覧回数
DipinPK
Contributor II

What is FIT image how to create FIT images for imx6 processors

0 件の賞賛
返信