Image shift right for LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image shift right for LVDS

1,397 Views
hankwang
Contributor V

Hi, I have a problem.  I use the sn65dsi8x dirver to enable LVDS signal. I can see the image, but image shift right.

I can modify which parameter to fix this problem ? I have tried the hfront_porch , hback_porch, but the problem is not fix.

S__24444930.jpg

Labels (1)
0 Kudos
Reply
2 Replies

988 Views
sabidi
Contributor I

Hi,

I'am working with imx8mm using sn65dsi83 and ihave the same issue, can you please share the solution?

0 Kudos
Reply

1,329 Views
igorpadykov
NXP Employee
NXP Employee

Hi hank

one can look at below variscite guidelines for adding custom panel. also

pay attention to proper panel initialization, function rad_panel_push_cmd_list() in

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

DART-MX8M Display - Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply