ISL79987 support with current SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISL79987 support with current SDK

ソリューションへジャンプ
1,299件の閲覧回数
mod42
Contributor III
I tried to port the patches in [1] to the current SDK (5.4.70_2.3.0) which we use on the 
iMX8QXP MEK (and on our custom hardware). But there is no function mxc_isi_initialize_capture_subdev 
which is called in 0001-ISI-Add-de-interlace-support.patch. So manually applying the patch is not 
possible. Is there a version of the patches for the current SDK?

[1
 
0 件の賞賛
返信
1 解決策
1,280件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I'm not aware of an update for this patch, but it could be used as reference to modify the ISI driver in newer releases like 5.4.70, the driver was moved from drivers/media/platform/imx8/ to drivers/staging/media/imx

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx?h=imx_5.4.70_2.3...

 

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,263件の閲覧回数
mod42
Contributor III

The patches didn't apply easily. I had to delay the porting to a later stage. We are currently in board bringup. But the ISL79987 driver works well and we can capture video. Deinterlacing is not as important as veryfying that the hardware works.

0 件の賞賛
返信
1,281件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I'm not aware of an update for this patch, but it could be used as reference to modify the ISI driver in newer releases like 5.4.70, the driver was moved from drivers/media/platform/imx8/ to drivers/staging/media/imx

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx?h=imx_5.4.70_2.3...

 

Best regards,
Aldo.

0 件の賞賛
返信