ISL79987 support with current SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISL79987 support with current SDK

Jump to solution
2,241 Views
mod42
Contributor III
I tried to port the patches in [1] to the current SDK (5.4.70_2.3.0) which we use on the 
iMX8QXP MEK (and on our custom hardware). But there is no function mxc_isi_initialize_capture_subdev 
which is called in 0001-ISI-Add-de-interlace-support.patch. So manually applying the patch is not 
possible. Is there a version of the patches for the current SDK?

[1
 
0 Kudos
Reply
1 Solution
2,222 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I'm not aware of an update for this patch, but it could be used as reference to modify the ISI driver in newer releases like 5.4.70, the driver was moved from drivers/media/platform/imx8/ to drivers/staging/media/imx

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx?h=imx_5.4.70_2.3...

 

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
2 Replies
2,205 Views
mod42
Contributor III

The patches didn't apply easily. I had to delay the porting to a later stage. We are currently in board bringup. But the ISL79987 driver works well and we can capture video. Deinterlacing is not as important as veryfying that the hardware works.

0 Kudos
Reply
2,223 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I'm not aware of an update for this patch, but it could be used as reference to modify the ISI driver in newer releases like 5.4.70, the driver was moved from drivers/media/platform/imx8/ to drivers/staging/media/imx

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/staging/media/imx?h=imx_5.4.70_2.3...

 

Best regards,
Aldo.

0 Kudos
Reply