IMX8m mini BD71847MWV RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8m mini BD71847MWV RTC

ソリューションへジャンプ
2,222件の閲覧回数
qiaoweibiao
Contributor III

I want to use the RTC of BD71847MWV  ,so i change the SCH to the below one.But it seems do not work correctly.PLS  HELP ME! Thanks a lot 

qiaoweibiao_0-1602991527680.png

qiaoweibiao_1-1602991570371.png

qiaoweibiao_2-1602991731744.png

 

 

 

0 件の賞賛
返信
1 解決策
2,198件の閲覧回数
qiaoweibiao
Contributor III
0 件の賞賛
返信
2 返答(返信)
2,201件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi QiangweiBiao,

For i.MX8MM RTC, if you want to keep the RTC clock after shutdown, it needs 2 voltages and a 32.768K clock:
1. NVCC_SNVS_1V8
2. VDD_SNVS_0V8
3. CLK_32K_OUT
Therefore, you need to check whether the output of LDO1 and LDO2 is normal and whether the output of C32K_OUT is normal after you remove 5V.

[In addition]
Considering that the power consumption of the RTC inside the CPU is larger than that of a separate RTC chip, it is strongly recommended that you use an independent RTC chip. NXP has many types of RTC chips, and you can choose one that meets your requirements.

 

Have a nice day!

B.R,

weidong

0 件の賞賛
返信
2,199件の閲覧回数
qiaoweibiao
Contributor III
 
0 件の賞賛
返信