imx6q hdmi compatible test fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q hdmi compatible test fail

2,809 次查看
jiangyaqiang
Senior Contributor I

HI anyone:

      Our project need to pass the "hdmi compatible test" but some item fail.

        Does anyone know about the hdmi CTS thing and give me a hand ?

      Here is the project information:

          1. hardware: imx6q

          2. software: android4.4.2 kernel:3.0.14

    fail items:

     1, 7-29, fail only on VIC1 640x480p 60Hz, the lab advise to change the N and CTS value according to the table, but I don't know where to modify :

  jiangyaqiang_0-1602469281268.png

  here is the log:

Test ID 7-29 : ACR

Verify N parameter value.
Found Audio Sample Packet
N Value = 0x1880
Pass
Verify CTS parameter value
Fs_actual = 39423.6005
CTS average = 31250.0000
Clock Accuracy (Bits 28,29) = [0x00]
Pass
Verify CTS transmitting interval
CTS interval = 0.00124292 Second
Error : Illegal CTS interval.
Test ID 7-29 : FAIL

 

fail 2:  7-13, C2 is too large on DUT OFF :

jiangyaqiang_1-1602469415820.png

 

 

 

 

0 项奖励
回复
5 回复数

2,799 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiangyaqiang

 

for supported HDMI timings one can refer to sect.33.4.3 Supported Video Mode

i.MX 6Dual/6Quad Applications Processor Reference Manual

and AN4671

AN4671, i.MX 6 Series HDMI Test Method for Eye Pattern and Electrical Characteristics - Application ...

 

Best regards
igor

0 项奖励
回复

2,763 次查看
jiangyaqiang
Senior Contributor I

HI igorpadykov: 

Thanks.

I have checked the video mode, it supports.

And the "Eye pattern" test is pass.

The test fail in CTS (hdmi compatible test), the fail item is :ID 7-29

and it only fail at resolution 640x480.

Here is the log:

(I have checked the N and CTS value, it's setted according toassociation provided, maybe the root cause is not the N and CTS value

)

--

Test ID 7-29 : ACR

 

Verify N parameter value.

Found Audio Sample Packet

N Value = 0x1880

Pass

Verify CTS parameter value

Fs_actual = 39423.6005

CTS average = 31250.0000

Clock Accuracy (Bits 28,29) = [0x00]

Pass

Verify CTS transmitting interval

CTS interval = 0.00124292 Second

Error : Illegal CTS interval.

Test ID 7-29 : FAIL

 

 

0 项奖励
回复

2,759 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiangyaqiang

 

for CTS tests may be suggested to proceed with extended support of

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 项奖励
回复

2,749 次查看
jiangyaqiang
Senior Contributor I

HI :

 

    But the "Professional Engineering Services" need to pay. 

    We don't want to pay for such an issue, the evk board should have did the test, could you contact your 

internal engeer, who have ever handle the CTS ?

0 项奖励
回复

2,745 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiangyaqiang

 

unfortunately there are no other standard ways for CTS tests support.

Suggest to apply to local marketing office to check if  it is possible to help with other options.

 

Best regards
igor

0 项奖励
回复