IMX8QXP drmModeGetResources failed (Operation not supported) REEOR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QXP drmModeGetResources failed (Operation not supported) REEOR

3,158 次查看
wang12zhe
Contributor III

environment


IMX8QXP EVK
Yocto:L5.10.35_2.0.0

I'm trying to run QT application on IMX8QXP EVK board,but get below error:
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~# ./TestVideo -platform eglfs
QML debugging is enabled. Only use this in a safe environment.
drmModeGetResources failed (Operation not supported)
Cannot create window: no screens available[ 494.233153] audit: type=1701 audit(1616582007.628:9): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=624 comm="TestVideo" exe="/home/root/TestVideo" sig=6 res=1

Aborted


root@imx8qxpmek:~# dmesg -c
[ 494.233153] audit: type=1701 audit(1616582007.628:9): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=624 comm="TestVideo" exe="/home/root/TestVideo" sig=6 res=1
root@imx8qxpmek:~#

please give me any suggestion,thanks very much

0 项奖励
回复
2 回复数

2,694 次查看
f1engmin11
Contributor I

@wang12zhe 
Excuse me, have your problem solved?    I met the same problem on imx8mmini  EVK . @Zhiming_Liu 

0 项奖励
回复

3,153 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@wang12zhe 

Do you try other drm card node?

0 项奖励
回复