v5.10.72-2.2.3_images_IMX6QPDLSOLOX Desktop view

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

v5.10.72-2.2.3_images_IMX6QPDLSOLOX Desktop view

559 Views
B_Prabhu
Contributor III

Hello,

I am using i.MX6DLSABRE_AI and flashed 5.10.72-2.2.3 BSP files, it is booting up there is no issue. My doubt is i can see only the terminal window in the HDMI monitor (see attachement), is that only option available in this BSP files? or something i have missed? how the windows look like in this version?

To enable frame buffer i have used below command in boot environment "setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'"

Could you please support me.

0 Kudos
Reply
3 Replies

518 Views
joanxie
NXP TechSupport
NXP TechSupport

did you use prebuit images? if yes, which image do you use?

0 Kudos
Reply

512 Views
B_Prabhu
Contributor III
0 Kudos
Reply

474 Views
joanxie
NXP TechSupport
NXP TechSupport

this demo images are built wayland as backend, if you need other backend, you need build by yourself, more detailed information, pls refer to the ycoto user guide

0 Kudos
Reply