IMX8QXP - Configuring A35 as RPMSG Slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP - Configuring A35 as RPMSG Slave

1,476件の閲覧回数
jithesh77
Contributor I

Hi 

Please confirm on the procedure IMX8QXP - Configuring A35 core as RPMSG Slave. I am planning to use M4 core as Master. Is it possible . Could you please confirm the procedure.

Thanks

Jithesh

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,460件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh

 

currently nxp linux bsps support only A35 as master (linux side), though seems in theory

it is possible to use A35 as slave. Also from rpmsg documentation on below link it is possible

to initiate transfer from slave side too:

https://www.programmersought.com/article/16266958328/

 

Best regards
igor

0 件の賞賛
返信

1,449件の閲覧回数
jithesh77
Contributor I

Hi Igor,

Thanks for the quick update .

Regarding Name Service Announce message, currently nxp linux bsps support  NS Announcement handling by default? . In my understanding linux side is supporting only dynamic channel creation through NS Announcements from remote core. Is my understanding correct ?

Is it possible to initiate NS Announcement from Slave M4 . Linux bsp accepts the Announcement from slave even if it act as RPMsg master. 

Could you please confirm.

Thanks

Jithesh

0 件の賞賛
返信