MCIMX6ULL-EVK and U-Boot hab_auth_image failures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6ULL-EVK and U-Boot hab_auth_image failures

688 Views
JohnKlug
Senior Contributor I

If I use Engine = SW, I see this result:

Authenticate image from DDR location 0x80800000...
data abort
pc : [<0000a8a2>]          lr : [<0000ab1f>]
reloc pc : [<e78c08a2>]    lr : [<e78c0b1f>]
sp : 9ef03460  ip : 0000e7ed     fp : 007b4fe0
r10: 10800000  r9 : 9ef0373c     r8 : 00000000
r7 : 00000000  r6 : 00904cb4     r5 : 10800000  r4 : 00000000
r3 : 5be0cd19  r2 : 00000008     r1 : 00904cb4  r0 : 10800000
Flags: nZCv  IRQs off  FIQs off  Mode SVC_32 (T)
Code: 2a08 d1ea 4605 2400 (f810) 7024 
Resetting CPU ...

If I use Engine = ANY, then I get both HAB_INV_ASSERTION and HAB_INV_SIGNATURE.

Keys:

Reading bank 3:

Word 0x00000000: f315b190 99ef27c6 26b10686 abdd61dc
Word 0x00000004: 9c001352 d2c95d64 6ce8e499 21f083c7

The keys I used are the same:

0xF315B190
0x99EF27C6
0x26B10686
0xABDD61DC
0x9C001352
0xD2C95D64
0x6CE8E499
0x21F083C7

I tried to follow HAB for Dummies.  https://boundarydevices.com/high-assurance-boot-hab-dummies/ 

Here are the first two errors:

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
        0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
        0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00
        0x00 0x00 0x02 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 2 -----------------
event data:
        0xdb 0x00 0x14 0x42 0x33 0x18 0xc0 0x00
        0xca 0x00 0x0c 0x00 0x01 0xc5 0x00 0x00
        0x00 0x00 0x07 0xdc

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)

 

 

 

0 Kudos
Reply
2 Replies

651 Views
JohnKlug
Senior Contributor I

I found out that for the i.MX6 ULL you must use Engine = SW.

 

Also, I was trying to use shadow registers (because of limited early board supply), but apparently they are ignored.

 

679 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply