IMX8QXP - Configuring A35 as RPMSG Slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP - Configuring A35 as RPMSG Slave

1,488 Views
jithesh77
Contributor I

Hi 

Please confirm on the procedure IMX8QXP - Configuring A35 core as RPMSG Slave. I am planning to use M4 core as Master. Is it possible . Could you please confirm the procedure.

Thanks

Jithesh

0 Kudos
Reply
2 Replies

1,472 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jithesh

 

currently nxp linux bsps support only A35 as master (linux side), though seems in theory

it is possible to use A35 as slave. Also from rpmsg documentation on below link it is possible

to initiate transfer from slave side too:

https://www.programmersought.com/article/16266958328/

 

Best regards
igor

0 Kudos
Reply

1,461 Views
jithesh77
Contributor I

Hi Igor,

Thanks for the quick update .

Regarding Name Service Announce message, currently nxp linux bsps support  NS Announcement handling by default? . In my understanding linux side is supporting only dynamic channel creation through NS Announcements from remote core. Is my understanding correct ?

Is it possible to initiate NS Announcement from Slave M4 . Linux bsp accepts the Announcement from slave even if it act as RPMsg master. 

Could you please confirm.

Thanks

Jithesh

0 Kudos
Reply