IMX8QM_spi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QM_spi

1,472件の閲覧回数
bzhang24
Contributor I

IMX8QM_kernel4.14_spi: the mosi, cs and sclk works well, if the miso is always low level, the miso sampled data is null or normal data that just is zero?

ラベル(1)
0 件の賞賛
返信
1 返信

1,392件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhang

if miso is low level then miso sampled data are zeros.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信