IMX8QM_spi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM_spi

1,492 Views
bzhang24
Contributor I

IMX8QM_kernel4.14_spi: the mosi, cs and sclk works well, if the miso is always low level, the miso sampled data is null or normal data that just is zero?

0 Kudos
Reply
1 Reply

1,412 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

if miso is low level then miso sampled data are zeros.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply