IMX8MP isp server does not dequeue frames?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP isp server does not dequeue frames?

1,721 次查看
nbi
Contributor I

I'm trying to figure out what goes wrong when streaming from a camera connected to the MIPI interface of the imx8mp.

I'm able to stream raw12 video data through the ISP, but for some reason after several "start/stop streaming", it stops working.

I have two issues.

1. MIPI data keeps flowing and I can see that the interrupts occur on the mipi interface. But there is no data passed to the ISP? If i set the format to 1080p then after ~1080 frames a frame will dequeue a .
If i run 640x480, a frame will dequeue after 480 frames:
video10: VIDIOC_DQBUF: 00:17:03.610752 index=0, type=vid-cap, request_fd=0, flags=0x00002001, field=none, sequence=0, memory=mmap, bytesused=614400, offset/userptr=0x0, length=614400

So it is somehow related to the image size.

(see log below)

[ 1031.733958] mxc-mipi-csi2.0: Frame Start: 19
[ 1031.738230] mxc-mipi-csi2.0: status: 01000000
[ 1031.754893] mxc-mipi-csi2.0: Frame End: 19
[ 1031.758989] mxc-mipi-csi2.0: status: 00100000
[ 1031.767295] mxc-mipi-csi2.0: Frame Start: 20
[ 1031.771567] mxc-mipi-csi2.0: status: 01000000
[ 1031.788247] mxc-mipi-csi2.0: Frame End: 20

...

[ 1021.729297] videodev: v4l2_poll: video10: poll: 00000000 000000fb
[ 1021.733472] mxc-mipi-csi2.0: Frame Start: 424

...

[ 1023.604813] mxc-mipi-csi2.0: Frame Start: 480
[ 1023.609171] mxc-mipi-csi2.0: status: 01000000
[ 1023.614254] video10: VIDIOC_DQBUF: 00:17:03.610752 index=0, type=vid-cap, request_fd=0, flags=0x00002001, field=none, sequence=0, memory=mmap, bytesused=614400, offset/userptr=0x0, length=614400
[ 1023.631617] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[ 1023.635497] mxc-mipi-csi2.0: Frame End: 480

 

2. No mipi interrupts! Everything looks like it should on the MIPI interface, but sometimes when I start a stream, the mipi intializes and starts as usual, but nothing happens afterwards, no MIPI interrupts. I've measured the power consumption on the camera, but it seems to be running as expected.

[ 1978.522978] mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0
[ 1978.528854] mxc-mipi-csi2.0: fmt: 0x2008, 640 x 480
[ 1978.551171] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[ 1978.556427] mxc-mipi-csi2.0: CSIS_VERSION[0]: 0x03060301
[ 1978.562452] mxc-mipi-csi2.0: CSIS_CMN_CTRL[4]: 0x00004905
[ 1978.568475] mxc-mipi-csi2.0: CSIS_CLK_CTRL[8]: 0x000f0000
[ 1978.574496] mxc-mipi-csi2.0: CSIS_INTMSK[10]: 0x0fffff1f
[ 1978.580602] mxc-mipi-csi2.0: CSIS_INTSRC[14]: 0x00000000
[ 1978.586708] mxc-mipi-csi2.0: CSIS_DPHYSTATUS[20]: 0x000000f1
[ 1978.592814] mxc-mipi-csi2.0: CSIS_DPHYCTRL[24]: 0x0d800007
[ 1978.598919] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_L[30]: 0x000001f4
[ 1978.605024] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_H[34]: 0x00000000
[ 1978.611132] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_L[38]: 0x00000000
[ 1978.617238] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_H[3c]: 0x00000000
[ 1978.623343] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH0[40]: 0x000000ac
[ 1978.629450] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH1[50]: 0x000008fd
[ 1978.635557] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH2[60]: 0x000008fe
[ 1978.641662] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH3[70]: 0x000008ff
[ 1978.647769] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH0[44]: 0x01e00280
[ 1978.653878] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH1[54]: 0x80008000
[ 1978.659987] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH2[64]: 0x80008000
[ 1978.666098] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH3[74]: 0x80008000
[ 1978.672214] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH0[48]: 0x00000000
[ 1978.678328] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH1[58]: 0x00000000
[ 1978.684435] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH2[68]: 0x00000000
[ 1978.690542] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH3[78]: 0x00000000
[ 1978.696650] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[ 1978.701888] mxc-mipi-csi2.0: GPR_GASKET_0_CTRL[60]: 0x00000000
[ 1978.707995] mxc-mipi-csi2.0: GPR_GASKET_0_HSIZE[64]: 0x00000000
[ 1978.714131] mxc-mipi-csi2.0: GPR_GASKET_0_VSIZE[68]: 0x00000000
[ 1978.720824] enter wdr3_hw_init

 

 

Any help is much appreciated.

标记 (5)
0 项奖励
回复
1 回复

1,654 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Would you provide more details, on how are you running the test?

Is it gstreamer pipeline?
Are you modifying the device tree?
Are you writing your test?

Please provide more details on how the issue can be reproduce it.

 

Regards

0 项奖励
回复