DDR frequency at CPU throttling due to temperature crosses passive temperature value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR frequency at CPU throttling due to temperature crosses passive temperature value

517 Views
roshanmohammed
Contributor I

We are using IMX6ULL processor.  We set the DDR frequency to 400 MHz and CPU frequency to 792 MHz. We observed that CPU clock frequency is reduced to 192 MHz during CPU throttling due to temperature crosses passive temperature value. During throttling what would be the DDR frequency change? 

Let us know what is the min DDR frequency supports during normal or throttling working condition. 

Labels (1)
0 Kudos
Reply
1 Reply

473 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @roshanmohammed,

I hope you are doing well
 
There is no such information regarding the DDR frequency due to CPU throttling. It mostly affects the CPU, GPU, and VPU.
 
For the DDR frequency information, please take a look at the sections Software Thermal Management Techniques and BUS Frequency Scaling from Document i.MX 6 Series Thermal Management Guidelines and section 2.5.4 Dynamic Bus Frequency from the i.MX Linux Reference Manual.
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply