IMX8MP hifi4 dsp codec library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP hifi4 dsp codec library

3,319 次查看
jiada
Contributor III

Hello NXP support team

We are evaluating hifi4 dsp on iMX8MP, so far we are able to compile DSP framework, unit-test, from imx-audio-framework , and confirmed hifi4 dsp can be started/stopped via sysfs interface

But executing of unit-test failed with error message

root@imx8mpevk:~# dsp_test.out -f1 -d16 -itest.mp3 -otest.pcm
****************************************************************
Cadence Audio Framework (Hostless) : 'Decoder'
Build: NON_XTENSA, RTOS: Linux, On: Jan 10 2023 23:53:16
Copyright (c) 2015-2020 Cadence Design Systems, Inc.
Lib Name : Audio Framework (Hostless)
Lib Version : 2.6
API Version : 2.0
****************************************************************
Audio Device Ready
xaf_load_library failed, Error code : -2 (invalid value at src/xaf-fsl-dec-test.c:513)

By looking at unit-test source code and  i.MX DSP User's Guide (nxp.com) 

I think this is because I am missing DSP codec and DSP codec wrapper libraries,
which needs authorization from NXP marketing or can be downloaded from yocto mirror server
(but so far I am not able to find where to download)

Could you please provide us required DSP codec and codec wrapper libraries
or let us know where to download?

DSP codec & wrapper library: (need authorization from NXP marketing)

/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_codec_wrap.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_mp3_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_aac_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_bsac_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_dabplus_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_drm_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_mp2_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_sbc_dec.so
/usr/lib/imx-mm/audio-codec/dsp/lib_dsp_sbc_enc.so
/usr/lib/imx-mm/audio-codec/dsp/lib_wma10d_wrap_dsp.so

DSP codec wrapper library: (can be downloaded from yocto mirror server)

/usr/lib/imx-mm/audio-codec/dsp/lib_mp3d_wrap_dsp.so
/usr/lib/imx-mm/audio-codec/dsp/lib_aacd_wrap_dsp.so
/usr/lib/imx-mm/audio-codec/dsp/lib_vorbisd_wrap_dsp.so
/usr/lib/imx-mm/audio-codec/dsp/lib_nbamrd_wrap_dsp.so
/usr/lib/imx-mm/audio-codec/dsp/lib_wbamrd_wrap_dsp.so

(listed in “7.2 Binary files in Linux OS rootfs” of i.MX DSP User's Guide (nxp.com) )

Thanks,
Jiada

标签 (1)
0 项奖励
回复
7 回复数

2,603 次查看
panpanjiangjiang
Contributor II

According to the i.MX DSP User's Guide documentation our problem was solved, thank you very much。

0 项奖励
回复

3,283 次查看
joanxie
NXP TechSupport
NXP TechSupport

I have already  mailed to you, pls check the mail

0 项奖励
回复

2,650 次查看
praveen_yaramada
Contributor II

Hi @joanxie , Can you also send me a copy of the NXP's codec library ? I am stuck in the similar fashion. I could not locate the libraries or the Yocto mirror site. My platform is also a iMX8 MP EVK.

Thankyou

0 项奖励
回复

2,616 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls create a new case for your request

0 项奖励
回复

2,704 次查看
panpanjiangjiang
Contributor II
Hi @joanxie
I have already resolved the previous issue, but now I want to integrate our own audio codec library because the desired codec protocol is not available. How can we integrate our own audio codec library into the DSP?
0 项奖励
回复

2,611 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you still have issue about this, pls create a new case for this, and uploaded detailed your use case information

0 项奖励
回复

2,940 次查看
mrjacob
Contributor I

Hi @joanxie 

I have mailed to you, pls check

Thanks.

0 项奖励
回复