IMX8MP - Use ISP auto exposure algorithm on external frames

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MP - Use ISP auto exposure algorithm on external frames

跳至解决方案
263 次查看
jheaffey
Contributor III

Hi,

I'm wondering if it is possible to use the auto exposure algorithm of the IMX8MP (the Vivante ISP8000) on video frames not sent from CSI MIPI interface? Specifically I would like to use the auto exposure algorithm if the ISP8000 on frames from an external camera.

 

The Verisilicon website states that the ISP supports "DMA Read Path to Feed Pipeline with Data from Memory" - https://www.verisilicon.com/en/IPPortfolio/VivanteISP8000

This post refers to the VSI SDK, perhaps this is what I need? I can't seem to find it though.

https://community.nxp.com/t5/i-MX-Processors/libcamera-on-imx8mp/m-p/1641491/highlight/true#M204952

0 项奖励
回复
1 解答
201 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it is possible but you need to do since not sample available, check this:

https://www.nxp.com/docs/en/user-guide/UG10168.pdf

 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
202 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it is possible but you need to do since not sample available, check this:

https://www.nxp.com/docs/en/user-guide/UG10168.pdf

 

Regards

0 项奖励
回复