IMX8MP - Use ISP auto exposure algorithm on external frames

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP - Use ISP auto exposure algorithm on external frames

Jump to solution
988 Views
jheaffey
Contributor III

Hi,

I'm wondering if it is possible to use the auto exposure algorithm of the IMX8MP (the Vivante ISP8000) on video frames not sent from CSI MIPI interface? Specifically I would like to use the auto exposure algorithm if the ISP8000 on frames from an external camera.

 

The Verisilicon website states that the ISP supports "DMA Read Path to Feed Pipeline with Data from Memory" - https://www.verisilicon.com/en/IPPortfolio/VivanteISP8000

This post refers to the VSI SDK, perhaps this is what I need? I can't seem to find it though.

https://community.nxp.com/t5/i-MX-Processors/libcamera-on-imx8mp/m-p/1641491/highlight/true#M204952

0 Kudos
Reply
1 Solution
925 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it is possible but you need to do since not sample available, check this:

https://www.nxp.com/docs/en/user-guide/UG10168.pdf

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
926 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it is possible but you need to do since not sample available, check this:

https://www.nxp.com/docs/en/user-guide/UG10168.pdf

 

Regards

0 Kudos
Reply