IMX8MP Ethernet Driver for Cortex M7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP Ethernet Driver for Cortex M7

ソリューションへジャンプ
2,799件の閲覧回数
Samhitha_Kashyap
Contributor III

Hello, 

I am writing a driver for ethernet Cortex M7 running on FreeRTOS

In the reference manual, Table 2-5. AIPS3 Memory Map states the base start address of the ENET is 0x30BE0000 and in the chapter 11.6.4.1.1 ENET memory map, the ENET base address: 4042_4000h.

https://www.nxp.com/webapp/Download?colCode=IMX8MPRM 

Can anyone help me understand the difference between the two base address?

Hardware used: Variscite IMX8MP carrier board with Co-processors Cortex A-53 and M-7

IMX8MPLUS 

ラベル(1)
0 件の賞賛
返信
1 解決策
2 返答(返信)
2,781件の閲覧回数
Samhitha_Kashyap
Contributor III

Thanks for the response!

0 件の賞賛
返信
2,788件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信