ENET memory map on iMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ENET memory map on iMX8MP

Jump to solution
3,257 Views
Hideo_Noda
Contributor I

Hi,

I have "i.MX 8M Plus Applications Processor Refernce Manual Rev.1 06/2021" here.

There are descriptions in 11.6.4.1.1 ENET memory map at page 3822, which describe

ENET base address: 4042_4000h

ENET1G base address: 4042_0000h

followed by the register map table.

I know that ENET registers are located at 0x30be0000 and 0x30bf0000 for eth0 and eth1 respectively.

What are the addresses 40424000h and 40420000h mentioned in the manual?

 

0 Kudos
Reply
1 Solution
3,251 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hideo

 

>What are the addresses 40424000h and 40420000h mentioned in the manual?

 

sorry this is misprint.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
3,247 Views
Hideo_Noda
Contributor I

igor,

 

Thank you.

I suspected so.

0 Kudos
Reply
3,252 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hideo

 

>What are the addresses 40424000h and 40420000h mentioned in the manual?

 

sorry this is misprint.

 

Best regards
igor

0 Kudos
Reply