IMX8MP Ethernet Driver for Cortex M7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP Ethernet Driver for Cortex M7

Jump to solution
2,886 Views
Samhitha_Kashyap
Contributor III

Hello, 

I am writing a driver for ethernet Cortex M7 running on FreeRTOS

In the reference manual, Table 2-5. AIPS3 Memory Map states the base start address of the ENET is 0x30BE0000 and in the chapter 11.6.4.1.1 ENET memory map, the ENET base address: 4042_4000h.

https://www.nxp.com/webapp/Download?colCode=IMX8MPRM 

Can anyone help me understand the difference between the two base address?

Hardware used: Variscite IMX8MP carrier board with Co-processors Cortex A-53 and M-7

IMX8MPLUS 

0 Kudos
Reply
1 Solution
2 Replies
2,868 Views
Samhitha_Kashyap
Contributor III

Thanks for the response!

0 Kudos
Reply