IMX8M Rebooting in every 5 seconds after setting display bootargs to HDMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8M Rebooting in every 5 seconds after setting display bootargs to HDMI

跳至解决方案
5,995 次查看
samad_meets
Contributor II

u-boot=> setenv bootargs console=ttymxc0,115200 earlycon=ec_imx6q0,0x0000000030860000,115200 init=/ init video=HDMI-A-1:1920x1080-32@60 androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale androidboot.fbTileSupport=enable cma=1536M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware

u-boot=> saveenv

Saving Environment to MMC... Writing to MMC(0)... OK


u-boot=> boot

verify OK, boot 'boot_a'
Kernel load addr 0x40480000 size 29089 KiB
kernel @ 40480000 (29786624)
ramdisk @ 43600000 (7425344)
fdt @ 43400000 (47520)
## Flattened Device Tree blob at 43400000
Booting using the fdt blob at 0x43400000
Using Device Tree in place at 0000000043400000, end 000000004340e99f

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.78-g1bb8d0d (root@367f7b2032d7) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #1 SMP PREEMPT Tue Apr 30 14:34:00 UTC 2019
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: TechNexion PICO-IMX8M and PI baseboard
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: ION carveout pool at 0x00000000f8000000, size 128 MiB
[ 0.000000] OF: reserved mem: initialized node imx_ion@0, compatible id imx-ion-pool
[ 0.000000] cma: Failed to reserve 1536 MiB
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xf7fb3200-0xf7fb4fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000ffffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x0000000097ffffff]
[ 0.000000] node 0: [mem 0x0000000098100000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000ffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] random: get_random_bytes called from start_kernel+0xa8/0x414 with crng_init=0
[ 0.000000] percpu: Embedded 25 pages/cpu @ffff8000b7f49000 s64792 r8192 d29416 u102400
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 773888
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q0,0x0000000030860000,115200 init=/ init video=HDMI-A-1:1920x1080-32@60 androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale androidboot.fbTileSupport=enable cma=1536M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware androidboot.serialno=191b09d6f060954c androidboot.btmacaddr=19:1b:09:d6:f0:60 androidboot.soc_type=imx8mq androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:500946,KL:0,KD:0,AVB:2147,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.verifiedbootstate=green androidboot.slot_suffix=_a dm="1 vroot none ro 1,0 3611944 verity 1 PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 4096 4096 451493 451493 sha1 6d97bc1edfe21ad7d6bd797d581b9e3a05145623 4a5cfee46b790c478ecf3b4abb23c48c10f85d10 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 fec_roo
[ 0.000000] device-mapper: init: will configure 1 devices
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 2934020K/3144704K available (14844K kernel code, 2336K rwdata, 6572K rodata, 5312K init, 529K bss, 210684K reserved, 0K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008f00000 ( 14848 KB)
[ 0.000000] .rodata : 0xffff000008f00000 - 0xffff000009570000 ( 6592 KB)
[ 0.000000] .init : 0xffff000009570000 - 0xffff000009aa0000 ( 5312 KB)
[ 0.000000] .data : 0xffff000009aa0000 - 0xffff000009ce8200 ( 2337 KB)
[ 0.000000] .bss : 0xffff000009ce8200 - 0xffff000009d6c780 ( 530 KB)
[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0003000000 ( 48 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff8000c0000000 ( 3072 MB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] i.MX8MQ clock driver init done
[ 0.000000] arch_timer: cp15 timer(s) running at 8.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.000921] system counter timer init
[ 0.000975] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.000985] clocksource: imx sysctr: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.002472] Console: colour dummy device 80x25
[ 0.002524] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333)
[ 0.002538] pid_max: default: 32768 minimum: 301
[ 0.002618] Security Framework initialized
[ 0.002629] SELinux: Initializing.
[ 0.004224] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[ 0.004975] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.005026] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.005057] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.019981] ASID allocator initialised with 32768 entries
[ 0.027987] Hierarchical SRCU implementation.
[ 0.036707] Cannot find MU entry in device tree
[ 0.036899] CPU identified as i.MX8MQ, silicon rev 2.0
[ 0.038106] EFI services will not be available.
[ 0.044041] smp: Bringing up secondary CPUs ...
[ 0.072238] Detected VIPT I-cache on CPU1
[ 0.072271] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.072309] CPU1: Booted secondary processor [410fd034]
[ 0.100307] Detected VIPT I-cache on CPU2
[ 0.100332] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.100363] CPU2: Booted secondary processor [410fd034]
[ 0.128401] Detected VIPT I-cache on CPU3
[ 0.128428] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.128459] CPU3: Booted secondary processor [410fd034]
[ 0.128687] smp: Brought up 1 node, 4 CPUs
[ 0.128719] SMP: Total of 4 processors activated.
[ 0.128728] CPU features: detected feature: GIC system register CPU interface
[ 0.128735] CPU features: detected feature: 32-bit EL0 Support
[ 0.128743] CPU features: detected feature: Kernel page table isolation (KPTI)
[ 0.158733] CPU: All CPU(s) started at EL2
[ 0.158908] alternatives: patching kernel code
[ 0.159276] CPU3: update max cpu_capacity 1024
[ 0.160416] devtmpfs: initialized
[ 0.160446] CPU1: update max cpu_capacity 1024
[ 0.171451] Registered cp15_barrier emulation handler
[ 0.171517] Registered setend emulation handler
[ 0.172368] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.172418] futex hash table entries: 1024 (order: 5, 131072 bytes)
[ 0.173169] pinctrl core: initialized pinctrl subsystem
[ 0.177049] DMI not present or invalid.
[ 0.177711] NET: Registered protocol family 16
[ 0.179584] schedtune: configured to support 5 boost groups
[ 0.184549] cpuidle: using governor menu
[ 0.186724] vdso: 2 pages (1 code @ ffff000008f07000, 1 data @ ffff000009aa4000)
[ 0.186740] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.187462] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.189177] Serial: AMBA PL011 UART driver
[ 0.198325] imx8mq-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver
[ 0.246608] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.258119] ACPI: Interpreter disabled.
[ 0.261834] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 45, base_baud = 1562500) is a IMX
[ 1.035147] console [ttymxc0] enabled
[ 1.039954] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 46, base_baud = 5000000) is a IMX
[ 1.049771] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 47, base_baud = 1562500) is a IMX
[ 1.059995] vgaarb: loaded
[ 1.063388] SCSI subsystem initialized
[ 1.068516] usbcore: registered new interface driver usbfs
[ 1.074177] usbcore: registered new interface driver hub
[ 1.080008] usbcore: registered new device driver usb
[ 1.093595] bd71837 0-004b: Device ID=0xA2
[ 1.097778] bd71837 0-004b: gpio_intr = 3
[ 1.101948] bd71837 0-004b: chip_irq=71
[ 1.118321] bd71837-pmic bd71837-pmic: regulator register name 'buck1'
[ 1.145572] bd71837-pmic bd71837-pmic: regulator register name 'buck2'
[ 1.172815] bd71837-pmic bd71837-pmic: regulator register name 'buck3'
[ 1.192033] bd71837-pmic bd71837-pmic: regulator register name 'buck4'
[ 1.211251] bd71837-pmic bd71837-pmic: regulator register name 'buck5'
[ 1.230464] bd71837-pmic bd71837-pmic: regulator register name 'buck6'
[ 1.249691] bd71837-pmic bd71837-pmic: regulator register name 'buck7'
[ 1.268908] bd71837-pmic bd71837-pmic: regulator register name 'buck8'
[ 1.288125] bd71837-pmic bd71837-pmic: regulator register name 'ldo1'
[ 1.315279] bd71837-pmic bd71837-pmic: regulator register name 'ldo2'
[ 1.330343] bd71837-pmic bd71837-pmic: regulator register name 'ldo3'
[ 1.357564] bd71837-pmic bd71837-pmic: regulator register name 'ldo4'
[ 1.384798] bd71837-pmic bd71837-pmic: regulator register name 'ldo5'
[ 1.412013] bd71837-pmic bd71837-pmic: regulator register name 'ldo6'
[ 1.439174] bd71837-pmic bd71837-pmic: regulator register name 'ldo7'
[ 1.478289] i2c i2c-0: IMX I2C adapter registered
[ 1.483081] i2c i2c-0: can't use DMA, using PIO instead.
[ 1.489582] i2c i2c-1: IMX I2C adapter registered
[ 1.494313] i2c i2c-1: can't use DMA, using PIO instead.
[ 1.500497] i2c i2c-2: IMX I2C adapter registered
[ 1.505227] i2c i2c-2: can't use DMA, using PIO instead.
[ 1.512408] media: Linux media interface: v0.10
[ 1.517053] Linux video capture interface: v2.00
[ 1.521868] pps_core: LinuxPPS API ver. 1 registered
[ 1.526910] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.536132] PTP clock support registered
[ 1.540350] EDAC MC: Ver: 3.0.0
[ 1.544147] dmi: Firmware registration failed.
[ 1.549953] MU is ready for cross core communication!
[ 1.555622] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 1.561397] imx rpmsg driver is registered.
[ 1.565818] Advanced Linux Sound Architecture Driver Initialized.
[ 1.572720] Bluetooth: Core ver 2.22
[ 1.576403] NET: Registered protocol family 31
[ 1.580866] Bluetooth: HCI device and connection manager initialized
[ 1.587241] Bluetooth: HCI socket layer initialized
[ 1.592197] Bluetooth: L2CAP socket layer initialized
[ 1.597298] Bluetooth: SCO socket layer initialized
[ 1.605634] clocksource: Switched to clocksource arch_sys_counter
[ 1.675249] VFS: Disk quotas dquot_6.6.0
[ 1.679257] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.686410] pnp: PnP ACPI: disabled
[ 1.700293] NET: Registered protocol family 2
[ 1.705339] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[ 1.713124] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[ 1.720469] TCP: Hash tables configured (established 32768 bind 32768)
[ 1.727186] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.733337] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.740082] NET: Registered protocol family 1
[ 1.747312] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.755842] kvm [1]: 8-bit VMID
[ 1.760319] kvm [1]: GICv3: no GICV resource entry
[ 1.765130] kvm [1]: disabling GICv2 emulation
[ 1.769709] kvm [1]: GIC system register CPU interface enabled
[ 1.775963] kvm [1]: vgic interrupt IRQ1
[ 1.780432] kvm [1]: Hyp mode initialized successfully
[ 1.794618] audit: initializing netlink subsys (disabled)
[ 1.800305] audit: type=2000 audit(1.707:1): state=initialized audit_enabled=0 res=1
[ 1.801400] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 1.816613] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.822831] Registering sdcardfs 0.1
[ 1.827170] fuse init (API version 7.26)
[ 1.831701] 9p: Installing v9fs 9p2000 file system support
[ 1.850016] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 1.857497] io scheduler noop registered
[ 1.861665] io scheduler cfq registered (default)
[ 1.866389] io scheduler mq-deadline registered
[ 1.870994] io scheduler kyber registered
[ 1.910810] imx-sdma 30bd0000.sdma: no iram assigned, using external mem
[ 1.917750] imx-sdma 30bd0000.sdma: Falling back to user helper
[ 1.929361] imx-sdma 302c0000.sdma: no iram assigned, using external mem
[ 1.946348] mxs-dma 33000000.dma-apbh: initialized
[ 1.955254] Bus freq driver module loaded
[ 1.962319] Config NOC for VPU and CPU
[ 1.973848] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.985526] SuperH (H)SCI(F) driver initialized
[ 1.991315] msm_serial: driver initialized
[ 2.003003] dcss-core 32e00000.dcss: Configured video pll 2 with ref_clk 1 freq 594000000 (actual 594000000)
[ 2.023939] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.030581] [drm] No driver support for vblank timestamp query.
[ 2.036723] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)
[ 2.044402] [drm] CDN_API_General_Test_Echo_Ext_blocking - APB(ret = 0 echo_resp = echo test)
[ 2.053006] [drm] CDN_API_General_getCurVersion - ver 13196 verlib 13062
[ 2.059768] [drm] Pixel clock frequency: 594000 KHz, character clock frequency: 594000, color depth is 8-bit.
[ 2.069761] [drm] Pixel clock frequency (594000 KHz) is supported in this color depth (8-bit). Settings found in row 27
[ 2.080560] [drm] VCO frequency is 5940000
[ 2.084735] [drm] VCO frequency (5940000 KHz) is supported. Settings found in row 14
[ 2.117499] [drm] CDN_API_General_Write_Register_blocking LANES_CONFIG ret = 0
[ 2.126897] [drm] hdmi-audio-codec driver bound to HDMI
[ 2.132156] imx-drm display-subsystem: bound 32c00000.hdmi (ops imx_hdp_imx_ops)
[ 2.139680] [drm] Cannot find any crtc or sizes
[ 2.144945] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[ 2.168723] brd: module loaded
[ 2.180759] loop: module loaded
[ 2.185067] zram: Added device: zram0
[ 2.201691] libphy: Fixed MDIO Bus: probed
[ 2.207600] NXP PHY: loading NXP PHY driver: [autonomous mode]
[ 2.214295] tun: Universal TUN/TAP device driver, 1.6
[ 2.219876] CAN device driver interface
[ 2.227161] fec 30be0000.ethernet: 30be0000.ethernet supply phy not found, using dummy regulator
[ 2.236938] pps pps0: new PPS source ptp0
[ 2.242617] random: fast init done
[ 2.242850] libphy: fec_enet_mii_bus: probed
[ 2.250469] mdio_bus 30be0000.ethernet-1: MDIO device at address 1 is missing.
[ 2.258855] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.265868] PPP generic driver version 2.4.2
[ 2.270673] PPP BSD Compression module registered
[ 2.275405] PPP Deflate Compression module registered
[ 2.280556] PPP MPPE Compression module registered
[ 2.285533] usbcore: registered new interface driver asix
[ 2.291205] usbcore: registered new interface driver ax88179_178a
[ 2.297472] usbcore: registered new interface driver cdc_ether
[ 2.303534] usbcore: registered new interface driver net1080
[ 2.309363] usbcore: registered new interface driver cdc_subset
[ 2.315509] usbcore: registered new interface driver zaurus
[ 2.321268] usbcore: registered new interface driver cdc_ncm
[ 2.335526] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.342104] ehci-pci: EHCI PCI platform driver
[ 2.346729] ehci-platform: EHCI generic platform driver
[ 2.352375] ehci-orion: EHCI orion driver
[ 2.356703] ehci-exynos: EHCI EXYNOS driver
[ 2.361226] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[ 2.367130] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.373344] ohci-pci: OHCI PCI platform driver
[ 2.377980] ohci-platform: OHCI generic platform driver
[ 2.383559] ohci-exynos: OHCI EXYNOS driver
[ 2.388756] Can't support > 32 bit dma.
[ 2.392660] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.398206] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 2.406041] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x01010810
[ 2.414836] xhci-hcd xhci-hcd.0.auto: irq 230, io mem 0x38200000
[ 2.421034] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.427867] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.435130] usb usb1: Product: xHCI Host Controller
[ 2.440028] usb usb1: Manufacturer: Linux 4.14.78-g1bb8d0d xhci-hcd
[ 2.446314] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 2.452216] hub 1-0:1.0: USB hub found
[ 2.456020] hub 1-0:1.0: 1 port detected
[ 2.460490] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.466008] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 2.473750] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 2.480560] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 2.487429] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.494670] usb usb2: Product: xHCI Host Controller
[ 2.499624] usb usb2: Manufacturer: Linux 4.14.78-g1bb8d0d xhci-hcd
[ 2.505909] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 2.511598] hub 2-0:1.0: USB hub found
[ 2.515400] hub 2-0:1.0: 1 port detected
[ 2.520627] usbcore: registered new interface driver usb-storage
[ 2.526819] usbcore: registered new interface driver usb_ehset_test
[ 2.533783] tusb320 1-0067: USB supply not found
[ 2.538539] tusb320 1-0067: select_mode: 0 dfp_power 0
[ 2.547942] tusb320 1-0067: device id: 023BSUT
[ 2.553362] tusb320 1-0067: reg08[0x00] , reg09[0xb0]
[ 2.562505] input: 30370000.snvs:snvs-powerkey as /devices/platform/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 2.574607] usbcore: registered new interface driver xpad
[ 2.580191] usbcore: registered new interface driver usb_acecad
[ 2.586348] usbcore: registered new interface driver aiptek
[ 2.592095] usbcore: registered new interface driver gtco
[ 2.597743] usbcore: registered new interface driver hanwang
[ 2.603634] usbcore: registered new interface driver kbtab
[ 2.613693] snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs-rtc-lp as rtc0
[ 2.623922] i2c /dev entries driver
[ 2.633823] ov5645_mipi 1-003c: 1-003c supply DOVDD not found, using dummy regulator
[ 2.641690] ov5645_mipi 1-003c: 1-003c supply DVDD not found, using dummy regulator
[ 2.649411] ov5645_mipi 1-003c: 1-003c supply AVDD not found, using dummy regulator
[ 2.725967] ov5645_mipi 1-003c: Read reg error: reg=300a
[ 2.731301] ov5645_mipi 1-003c: Camera is not found
[ 2.737992] mxc-mipi-csi2_yav 30a70000.mipi_csi1: mipi_csi2_probe
[ 2.744230] CSI: Registered sensor subdevice: mxc-mipi-csi2.0
[ 2.750014] mxc-mipi-csi2_yav 30a70000.mipi_csi: Remote device at /mipi_csi1@30a70000/port/endpoint1 XXX found
[ 2.760062] mxc-mipi-csi2_yav 30a70000.mipi_csi1: lanes: 2, name: mxc-mipi-csi2.0
[ 2.767998] mxc-mipi-csi2_yav 30b60000.mipi_csi2: mipi_csi2_probe
[ 2.774202] CSI: Registered sensor subdevice: mxc-mipi-csi2.1
[ 2.780042] mxc-mipi-csi2_yav 30b60000.mipi_csi: Remote device at /mipi_csi2@30b60000/port/endpoint1 XXX found
[ 2.790071] mxc-mipi-csi2_yav 30b60000.mipi_csi2: lanes: 2, name: mxc-mipi-csi2.1
[ 2.799557] usbcore: registered new interface driver uvcvideo
[ 2.805326] USB Video Class driver (1.1.1)
[ 2.811410] __power_supply_register: Expected proper parent device for 'battery'
[ 2.819150] (NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
[ 2.831535] __power_supply_register: Expected proper parent device for 'usb'
[ 2.843523] imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)
[ 2.851529] device-mapper: uevent: version 1.0.3
[ 2.856842] device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: dm-devel@redhat.com
[ 2.865960] Bluetooth: HCI UART driver ver 2.3
[ 2.870428] Bluetooth: HCI UART protocol H4 registered
[ 2.875643] Bluetooth: HCI UART protocol BCSP registered
[ 2.880974] Bluetooth: HCI UART protocol ATH3K registered
[ 2.886448] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.893061] Bluetooth: HCI UART protocol Broadcom registered
[ 2.898800] Bluetooth: HCI UART protocol QCA registered
[ 2.904394] bt power gpio is:85
[ 2.907778] rfkill: BT RF going to : on
[ 2.909667] mxc_bt_rfkill driver success loaded
[ 2.916544] rfkill: BT power going to : 1
[ 2.921437] sdhci: Secure Digital Host Controller Interface driver
[ 2.927639] sdhci: Copyright(c) Pierre Ossman
[ 2.932388] Synopsys Designware Multimedia Card Interface Driver
[ 2.940331] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.994763] mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA
[ 3.050267] mmc1: SDHCI controller on 30b50000.usdhc [30b50000.usdhc] using ADMA
[ 3.062567] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 3.068896] Galcore version 6.2.4.163672
[ 3.073347] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.080514] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.087732] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.094901] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.102118] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.109276] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.110636] mmc0: new HS400 MMC card at address 0001
[ 3.111358] mmcblk0: mmc0:0001 M52516 14.3 GiB
[ 3.111813] mmcblk0boot0: mmc0:0001 M52516 partition 1 4.00 MiB
[ 3.112252] mmcblk0boot1: mmc0:0001 M52516 partition 2 4.00 MiB
[ 3.112701] mmcblk0rpmb: mmc0:0001 M52516 partition 3 4.00 MiB
[ 3.120763] mmc1: queuing unknown CIS tuple 0x01 (3 bytes)
[ 3.123228] Alternate GPT is invalid, using primary GPT.
[ 3.123291] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 3.130534] mmc1: queuing unknown CIS tuple 0x1a (5 bytes)
[ 3.134502] mmc1: queuing unknown CIS tuple 0x1b (8 bytes)
[ 3.135295] mmc1: queuing unknown CIS tuple 0x14 (0 bytes)
[ 3.163878] mmc1: queuing unknown CIS tuple 0x80 (1 bytes)
[ 3.164097] mmc1: queuing unknown CIS tuple 0x81 (1 bytes)
[ 3.164315] mmc1: queuing unknown CIS tuple 0x82 (1 bytes)
[ 3.164400] mmc1: new ultra high speed SDR104 SDIO card at address 0001
[ 3.165785] [drm] Cannot find any crtc or sizes
[ 3.206241] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.213402] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.220620] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.227801] galcore 38000000.gpu: Cannot do DMA to address 0x0000000000000000
[ 3.257106] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 1
[ 3.269179] hantrodec: module inserted. Major = 235
[ 3.276316] ALL
[ 3.278246] ALL 0
[ 3.280174] ALL 1
[ 3.282143] ALL 2
[ 3.284071] ALL 2
[ 3.286073] ALL 2
[ 3.288001] ALL 2
[ 3.289943] ALL 2
[ 3.291871] ALL 2
[ 3.293871] ALL 2
[ 3.295799] ALL 2
[ 3.297740] ALL 2
[ 3.299669] ALL 2
[ 3.301596] ALL 2
[ 3.303537] ALL 2
[ 3.305464] ALL 2
[ 3.307406] ALL 2
[ 3.309333] ALL 2
[ 3.311299] ALL 2
[ 3.313227] ALL 3
[ 3.320552] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.329157] caam-snvs 30370000.caam-snvs: can't get snvs clock
[ 3.335149] caam-snvs 30370000.caam-snvs: violation handlers armed - init state
[ 3.343361] hidraw: raw HID events driver (C) Jiri Kosina
[ 3.351872] usbcore: registered new interface driver usbhid
[ 3.357541] usbhid: USB HID core driver
[ 3.393728] ashmem: initialized
[ 3.404033] usbcore: registered new interface driver snd-usb-audio
[ 3.420581] imx_sph0645_probe(): imx_sph0645_probe
[ 3.425506] imx_sph0645_probe(): Found 1 codec(s)
[ 3.430246] tfa_devm_kstrdup():
[ 3.433494] imx_sph0645_probe(): Reference clock found: sai3 @ 24576000
[ 3.440354] imx_sph0645_init():
[ 3.443705] imx-sph0645 sound-sph0645: sph0645 <-> 308c0000.sai mapping ok
[ 3.450668] imx-sph0645 sound-sph0645: ASoC: no DMI vendor name!
[ 3.457556] imx_sph0645_probe(): done
[ 3.461860]
[ 3.463405] Found 2 codec(s)
[ 3.466319]
[ 3.467827]
[ 3.469338] Reference clock found: sai2 @ 24576000
[ 3.474167] imx-tfa98xx sound-tfa9912: ASoC: CODEC DAI tfa98xx-aif-1-34 not registered
[ 3.482107] imx-tfa98xx sound-tfa9912: snd_soc_register_card failed (-517)
[ 3.488998] done
[ 3.492683] imx-cdnhdmi sound-hdmi: i2s-hifi <-> 30050000.sai mapping ok
[ 3.499430] imx-cdnhdmi sound-hdmi: ASoC: no DMI vendor name!
[ 3.507373] NET: Registered protocol family 26
[ 3.511846] u32 classifier
[ 3.514570] Actions configured
[ 3.517997] Netfilter messages via NETLINK v0.30.
[ 3.523055] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 3.529454] ctnetlink v0.93: registering with nfnetlink.
[ 3.535491] xt_time: kernel timezone is -0000
[ 3.539973] IPv4 over IPsec tunneling driver
[ 3.545009] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.552488] arp_tables: arp_tables: (C) 2002 David S. Miller
[ 3.559353] Initializing XFRM netlink socket
[ 3.564433] NET: Registered protocol family 10
[ 3.574802] Segment Routing with IPv6
[ 3.578561] mip6: Mobile IPv6
[ 3.581544] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 3.589796] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.597132] NET: Registered protocol family 17
[ 3.601707] NET: Registered protocol family 15
[ 3.606172] can: controller area network core (rev 20170425 abi 9)
[ 3.612477] NET: Registered protocol family 29
[ 3.616945] can: raw protocol (rev 20170425)
[ 3.621234] can: broadcast manager protocol (rev 20170425 t)
[ 3.626917] can: netlink gateway (rev 20170425) max_hops=1
[ 3.632867] Bluetooth: RFCOMM TTY layer initialized
[ 3.637772] Bluetooth: RFCOMM socket layer initialized
[ 3.643001] Bluetooth: RFCOMM ver 1.11
[ 3.646776] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.652104] Bluetooth: BNEP filters: protocol multicast
[ 3.657351] Bluetooth: BNEP socket layer initialized
[ 3.662334] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.668273] Bluetooth: HIDP socket layer initialized
[ 3.673255] lib80211: common routines for IEEE802.11 drivers
[ 3.679373] 9pnet: Installing 9P2000 support
[ 3.686267] registered taskstats version 1
[ 3.702694] hantro receive hot notification event: 0
[ 3.707695] cpu cpu0: registered imx8mq-cpufreq
[ 3.714210]
[ 3.715755] Found 2 codec(s)
[ 3.718658]
[ 3.720158]
[ 3.721677] Reference clock found: sai2 @ 24576000
[ 3.726492] imx-tfa98xx sound-tfa9912: ASoC: CODEC DAI tfa98xx-aif-1-34 not registered
[ 3.734423] imx-tfa98xx sound-tfa9912: snd_soc_register_card failed (-517)
[ 3.741306] done
[ 3.744854] input: gpio_keys as /devices/platform/gpio_keys/input/input1
[ 3.753242]
[ 3.754755] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:08:25 UTC (505)
[ 3.755568] usb_otg_vbus: disabling
[ 3.755571] backlight_pwr: disabling
[ 3.755574] wifi_vbus: disabling
[ 3.755577] wifi_sdio_vbus: disabling
[ 3.755587] ALSA device list:
[ 3.755589] #0: SPH0645
[ 3.755591] #1: imx-audio-hdmi
[ 3.786976] Found 2 codec(s)
[ 3.789875]
[ 3.791375]
[ 3.792879] Reference clock found: sai2 @ 24576000
[ 3.797802] imx-tfa98xx sound-tfa9912: ASoC: CODEC DAI tfa98xx-aif-1-34 not registered
[ 3.805732] imx-tfa98xx sound-tfa9912: snd_soc_register_card failed (-517)
[ 3.812669] done
[ 3.815085] device-mapper: init: attempting early device configuration.
[ 3.824156] device-mapper: init: adding target '0 3611944 verity 1 PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 4096 4096 451493 451493 sha1 6d97bc1edfe21ad7d6bd797d581b9e3a05145623 4a5cfee46b790c478ecf3b4abb23c48c10f85d10 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=1370056c-16ca-4a06-8455-00f44b5be475 fec_roots 2 fec_blocks 455050 fec_start 455050'
[ 3.872409] device-mapper: init: dm-0 is ready
[ 3.888348] EXT4-fs (dm-0): mounted filesystem without journal. Opts: (null)
[ 3.895455] VFS: Mounted root (ext4 filesystem) readonly on device 252:0.
[ 3.905123] devtmpfs: mounted
[ 3.909699] Freeing unused kernel memory: 5312K
[ 3.914332] Kernel panic - not syncing: Requested init / failed (error -13).
[ 3.921382] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.14.78-g1bb8d0d #1
[ 3.928167] Hardware name: TechNexion PICO-IMX8M and PI baseboard (DT)
[ 3.934693] Call trace:
[ 3.937146] [<ffff00000808b2fc>] dump_backtrace+0x0/0x414
[ 3.942545] [<ffff00000808b724>] show_stack+0x14/0x1c
[ 3.947598] [<ffff000008eca60c>] dump_stack+0x90/0xb0
[ 3.952650] [<ffff0000080dc21c>] panic+0x140/0x2ac
[ 3.957443] [<ffff000008edf6d8>] kernel_init+0xe4/0x140
[ 3.962669] [<ffff000008085064>] ret_from_fork+0x10/0x18
[ 3.967983] SMP: stopping secondary CPUs
[ 3.972433] Kernel Offset: disabled
[ 3.975920] CPU features: 0x080200c
[ 3.979406] Memory Limit: none
[ 3.982463] Rebooting in 5 seconds...

Dear NXP comrades,

I have flashed Android Pie image with support for 1920X1080 HDMI on my IMX8M-4G-DEV board

I am facing an issue in booting even after setting the bootargs in the u-boot mode.

Please help me with the same. I shall be grateful for the extended support.

Regards,

Abdus Samad

标签 (1)
标记 (1)
1 解答
4,716 次查看
mahi
Contributor IV

Looks like the kernel doesn't find init and in the bootargs, there is a space in between "init=/" and "init", which would explain the error...

Remove that space.

在原帖中查看解决方案

4 回复数
4,716 次查看
nguyentd3
Contributor II

You should attach U-Boot's Environment settings to this ticket for checking: 

Use below command to show all setting in in U-Boot:

$ printenv

As your booting logs, it don't see any settings for  root=/dev/mmcblk0pX

   X may be in below partitions:

p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15

Regards,

Nguyen

0 项奖励
回复
4,716 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdus

"Kernel panic" may be caused by ddr errors, so one can run ddr test

i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 

and and rebuild image using Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf included in package.

Then try with linux minimal image

linux-imx - i.MX Linux kernel 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,716 次查看
samad_meets
Contributor II

Thanks, igorpadykov‌ and mahi for a quick response.

One additional query, the development successfully booted Android GUI on Dell Monitor supporting the 1920x1080 resolution.

But what if I want to redirect the same display to 4K display? If possible, please let me know by doing some nominal changes.

0 项奖励
回复
4,717 次查看
mahi
Contributor IV

Looks like the kernel doesn't find init and in the bootargs, there is a space in between "init=/" and "init", which would explain the error...

Remove that space.