IMX8M Plus | Use UART3 (on J21)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Plus | Use UART3 (on J21)

Jump to solution
2,328 Views
shai_b
Senior Contributor II

Dear team,

My customer would like to use UART3 on the iMX8M Plus EVK, can you advise if the customer would like the use UART3 on J21 if he needs to change something in the device tree.

BTW, he still wants to debug via the USB port but he wants to add external UART communicate 

Waiting for your kind feedback, Thanks in advance

B.Regards,

Shai

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
2,320 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

View solution in original post

0 Kudos
Reply
2 Replies
2,321 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

0 Kudos
Reply
2,315 Views
shai_b
Senior Contributor II

@Zhiming_Liu,

Thanks for the input, it works out of the box as you said.

Just noting, you should enable UART3 for all imx8m EVK for example the EVK of the imx8m mini/nano does not come with UART3 enabled in the DTS and I think it should be enabled.

KR,

Shai

0 Kudos
Reply