IMX8M Plus | Use UART3 (on J21)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Plus | Use UART3 (on J21)

ソリューションへジャンプ
2,326件の閲覧回数
shai_b
Senior Contributor II

Dear team,

My customer would like to use UART3 on the iMX8M Plus EVK, can you advise if the customer would like the use UART3 on J21 if he needs to change something in the device tree.

BTW, he still wants to debug via the USB port but he wants to add external UART communicate 

Waiting for your kind feedback, Thanks in advance

B.Regards,

Shai

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,318件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,319件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

0 件の賞賛
返信
2,313件の閲覧回数
shai_b
Senior Contributor II

@Zhiming_Liu,

Thanks for the input, it works out of the box as you said.

Just noting, you should enable UART3 for all imx8m EVK for example the EVK of the imx8m mini/nano does not come with UART3 enabled in the DTS and I think it should be enabled.

KR,

Shai

0 件の賞賛
返信