IMX8M Plus | Use UART3 (on J21)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8M Plus | Use UART3 (on J21)

跳至解决方案
2,321 次查看
shai_b
Senior Contributor II

Dear team,

My customer would like to use UART3 on the iMX8M Plus EVK, can you advise if the customer would like the use UART3 on J21 if he needs to change something in the device tree.

BTW, he still wants to debug via the USB port but he wants to add external UART communicate 

Waiting for your kind feedback, Thanks in advance

B.Regards,

Shai

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
2,313 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,314 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @shai_b 

We have enabled uart3 in dts, customer can use it directly.

Regards

Zhiming

0 项奖励
回复
2,308 次查看
shai_b
Senior Contributor II

@Zhiming_Liu,

Thanks for the input, it works out of the box as you said.

Just noting, you should enable UART3 for all imx8m EVK for example the EVK of the imx8m mini/nano does not come with UART3 enabled in the DTS and I think it should be enabled.

KR,

Shai

0 项奖励
回复