IMX8M PLUS || PCIe Interface || Clock Type

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M PLUS || PCIe Interface || Clock Type

9,954件の閲覧回数
JyotiVaishnav
Contributor II

Hello NXP Team, 

I want to know the information regarding the PCIe clock of IMX8M PLUS processor. 

The PCIe Switch having which type of reference clock source. 

0 件の賞賛
返信
8 返答(返信)

9,937件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

This is the frequency requirement,

josephlinares_0-1698713033652.pngjosephlinares_0-1698713033652.png

The requirements are complient with the PCI specification as mentioned in the datasheet but you can have a reference is the design and device of 8M Plus' PCI reference clock generator.

Page 10 of schematic.

And 9FGV0241AKLF datasheet.

Regards

0 件の賞賛
返信

9,923件の閲覧回数
JyotiVaishnav
Contributor II

Hello @JosephAtNXP 

The external clock generator is necessary to use. 

We are not planning to use.  

 

0 件の賞賛
返信

9,916件の閲覧回数
JyotiVaishnav
Contributor II

Hello @JosephAtNXP 

Could you please brief about the purposes of using external PCIe clock generator used in the EVK board.

In our design we are planning to avoid external clock generator(9FGV0241AKLF) due to BOM optimization. So IMX 8M plus will act as a root complex device. So what will be the clock type from NXP processor?

and can we meet the standard PCIe clock requirement for the PCIe gen3.0 x1 Lane interface without using the external PCIe clock generator?

0 件の賞賛
返信

9,895件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

This piece of information is from 8M Plus' reference manual:

The PLL in the CMN synthesizes high-speed clock, which is used for TX serializer and RX CDR lock, from a reference clock. The reference clock can be selected from two clock sources; internal SoC reference clock and external differential reference clock.

In the PCIe PHY, the high frequency clock from PLL is used in the serialization of TX data and CDR lock acquisition and maintenance.

You can optimize BOM and use the internal oscillator, the main reason to use an external oscillator is to have the same reference for both PCI EP and RC's CDR. So, it can be traded off.

Regards,

0 件の賞賛
返信

9,836件の閲覧回数
Christo
Contributor II

Hi @JosephAtNXP , 

Termination/differential signal standard used in MIMX8ML6CVNKZAB

We are interfacing NXP with a PCIe switch(PI7C9X3G606GPBFCA) without using external clock generator. 

So, what will be the differential signal standard? is it HCSL?
And is it required to provide any kind of termination at driver side(NXP)? 
Can we get some reference document to know the differential clock type used? 

For providing the termination at endpoint(PCIe Switch) we need to know the more information about the differential clock type available at the source(NXP i.MX 8M Plus) side. Please guide to us. 

0 件の賞賛
返信

9,813件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Here are the guidelines provided by the hardware developers guide:

josephlinares_0-1699384091020.pngjosephlinares_0-1699384091020.png

josephlinares_1-1699384094192.pngjosephlinares_1-1699384094192.png

And this is a backup found in hardware developers guide:

On EVK, a PCIE clock generator chip (9FGV0241) is used to feed high-quality clock to both the PHY and connecter/device. If a PCIE clock generator is not available, use the internal clock of the chip. Note that the internal clock exhibits larger jitter than that from PCIE clock generator

These are guidelines from a PCIe training:

Layout and Routing Guidelines based on 8Gbps rules:


− AC coupling caps placed symmetrically? Near one end of the
channel?
− AC coupling caps located near TX end when connector is
implemented in system
− TX and RX data and REFCLKs routed as diff pairs
− Diff pairs routed symmetrically?
− No stubs anywhere in the diff pair routing
− No routing over plane splits or anti-pads
− Oblique routing used for diff pairs
− Diff pair (P-N) matching to within 10 mils for TX and RX data diff
pairs
− Diff pair (P-N) matching to within 5 mil for REFCLK diff pairs
− Max length of all diff pairs on add-in card < 4 inches
− Diff pair length matching near the location of mismatch; within
guidelines for sectional jogs?
− Lane-to-lane skew within tolerance
− Serpentine bends within guideline (no sharp angles)

Regards,

0 件の賞賛
返信

9,786件の閲覧回数
Christo
Contributor II

Hi @JosephAtNXP 

Attaching our use case. 
Use CaseUse Case

1) So which PCIe clock method is suggesting for us based on our use case? 
PCIe ClockPCIe Clock 

2) Which termination is suggesting for the PCIe clock? 
Our concern about the clock is if we proceed with the method 2, then need to know about the clock type...then only we can provide corresponding clock termination/transformations. Refer the attached application note for this query. 

0 件の賞賛
返信

9,772件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

As said, you can use internal clock or external clock in any application just considering that there may be a larger jitter, this increment can be in any application, and as you may see in schematics, there are no clock termination requirement, check that if internal clock'd be used, map M2 pins to processor pins.

josephlinares_0-1699568457501.pngjosephlinares_0-1699568457501.png

Regards,

0 件の賞賛
返信