IMX8M Mini A53 core UART debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Mini A53 core UART debug

2,652件の閲覧回数
suhas_mv
Contributor II

Hi,

We are using i.MX8M mini (MIMX8MM3CVTKZAA) in our design, when referred to i.MX8M mini EVK schematics (SPF-31399_C2), UART 2 is used for A53 debug and UART 4 is used for M4 debug, is it mandatory to use the same UART's for  A53 debug and M4 debug? Is it possible to move the debug ports to other UART's (i.e. UART 1 and UART 3)?

Regards,

Suhas

0 件の賞賛
返信
2 返答(返信)

2,640件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi suhas_mv

 

in general yes - it is possible to move the debug ports to other UART's

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm-evk.d...

Software changes may be performed for console (uart2) in dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm-evk.d...

 

Best regards
igor

 

0 件の賞賛
返信

2,617件の閲覧回数
suhas_mv
Contributor II

Thanks for the information

Regards,

Suhas

0 件の賞賛
返信