IMX8M Dual MIPI Display resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Dual MIPI Display resolution

2,692 Views
eren1
Contributor I

I have a 4 lane MIPI 1920x1200 resolution LCD and will start a new design with IMX8M Dual. In datasheet dispaly interface option is as follows.

MIPI-DSI Display Interface:
• MIPI-DSI 4 channels supporting one display, resolution up to 1920 x 1080 at 60 Hz.

Is it possible to use 1920x1200 resolution LCD in this design?  What will be the effect if I use this LCD. 

Labels (1)
0 Kudos
Reply
6 Replies

2,684 Views
joanxie
NXP TechSupport
NXP TechSupport

yes can support 1920x1200 mipi display

0 Kudos
Reply

2,679 Views
eren1
Contributor I

Will it be in full functionality, or do i need to apply low fps to catch full resolution?

 

0 Kudos
Reply

2,647 Views
joanxie
NXP TechSupport
NXP TechSupport

what frame rate do you need?

0 Kudos
Reply

2,631 Views
eren1
Contributor I

I need at least 50 fps. I wonder about the performance in 60 fps while driving 1200 columns instead of 1080. Will this mismatch cause an effect or flickering on image? I planned lowering fps to 50 to prevent any effect on image. I will need at least 50 fps to catch better user experience in page swiping and video performance.

Will the design be ok with 50 fps? Or off course it will be perfect if there is no problem in 60 fps.

0 Kudos
Reply

2,608 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the  i.MX 8MQ reference manual, The MIPI-DSI output resolution is supported up to 1920x1080@60 or 1800x1200@60

joanxie_0-1709715581684.png

so if you need 1920x1200 resolution, couldn't reach 60fps, 50fps should be ok

 

0 Kudos
Reply

2,495 Views
eren1
Contributor I

OK, thank you for your support.

0 Kudos
Reply