IMX8 imx-image-full qt5 pkg connection issue with VPN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 imx-image-full qt5 pkg connection issue with VPN

Jump to solution
2,041 Views
lchen
Contributor III

Hi,

I have successfully build imx-image-multimedia image for imx8qmmek. When I built imx-image-full image or SDK, the qt related pkgs always stuck at do_fetch job if my building machine is connected to company VPN. If I disconnect VPN and just use home network, the qt pkgs fetching works fine.

Is it because company firewall is blocking qt5 source? I can access the qt5 github from the browser.

Thanks,

Lijun

0 Kudos
Reply
1 Solution
2,027 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
2,036 Views
lchen
Contributor III

Never mind, I retried and passed this time.

0 Kudos
Reply
2,028 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

(y)

 

0 Kudos
Reply